Send an End of Schedule report

Send an End of Schedule report for a scheduled operation summary.
Prerequisites
  • To send schedule results, you must have
    Command a schedule and Edit a schedule
    permissions.
To send an End of Schedule report
  1. Select
    View > Schedules
    , or click the
    Schedules
    button.
  2. On the
    Schedules
    tab, click in the desired schedule's
    Completion Email List
    field and then click browse_button_small. The schedule must be inactive to change the email address, that is, the
    Active
    check box must be cleared.
  3. Complete the
    Contacts and Groups
    dialog box.
  4. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal