About sending schedule results

You can send two different types of schedule reports to specified recipients when a schedule completes. You can send an End of Schedule report that summarizes the operations completed during the schedule. You can also send a more detailed operation report (such as a Backup report or a Backup and Compare report) through an asset's scheduled operation properties.
End of Schedule report summarizes information such as a Backup and Compare schedule's start and stop times and whether there were any differences between the contents of the physical device and the asset's master file stored in the Archive.
Operation-specific report is a more detailed report regarding an asset's scheduled operation. For example, you can send a Backup report or a Backup and Compare report that includes information such as the asset and hardware details, the agent computer that ran the schedule, and the name and location of the master file used in a Compare. For Backup and Compare reports, you can also attach a Compare Report file to the email notification.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal