Device parameters for Rockwell Automation Compare

The lower right hand pane of the Rockwell Automation Compare Viewer contains settings for comparing the following devices. While comparisons can be conducted for Allen-Bradley PanelView Plus, Allen-Bradley MobileView devices, Asset Inventory, Allen-Bradley Stratix Switch, and FactoryTalk View Site Edition, no settings are available for them so these asset types are not included in this list.
Allen-Bradley MicroLogix Controller
These settings apply only to MicroLogix 1000 controllers. For MicroLogix 1100 and higher, a binary compare is conducted and no parameters are required. This compare tells you only whether or not there are differences, but gives no details.
  • Data Table Compare
    By default, all data table files are included in the compare. To select which data table files are compared (or turn off data table file comparison) click the field, and then click browse_button_small. Complete the
    Data Files Compare Options
    dialog box.
  • Program Compare
    By default, all program files are compared. To select which program files are compared (or turn off program file comparison) click the field, and then click browse_button_small. Complete the
    Program File Compare Options
    dialog box.
Allen-Bradley PLC-5 Controller
  • Compare Force Table
    Select
    True
    to include the controller's force values during the compare operation. Select
    False
    to exclude force values.
  • Data Table Compare
    By default, all data table files are included in the compare. To select which data table files are compared (or turn off data table file comparison) click the field, and then click browse_button_small. Complete the
    Data Files Compare Options
    dialog box.
    You must have RSLogix 5 programming software installed on the FactoryTalk AssetCentre client computer to configure this setting.
  • Program Compare
    By default, all program files are compared. To select which program files are compared (or turn off program file comparison) click the field, and then click browse_button_small. Complete the
    Program File Compare Options
    dialog box.
    You must have RSLogix 5 programming software installed on the FactoryTalk AssetCentre client computer to configure this setting.
RA Drive
  • Compare All
    Select
    True
    to compare all data fields within a file. Select
    False
    to compare only editable fields within a file.
Allen-Bradley SLC 500 Controller
You must have RSLogix 500 programming software installed on the FactoryTalk AssetCentre client computer to configure these settings.
  • Data Table Compare
    By default, all data table files are included in the compare. To select which data table files are compared (or turn off data table file comparison) click the field, and then click browse_button_small. Complete the
    Data Files Compare Options
    dialog box.
  • Program Compare
    By default, all program files are compared. To select which program files are compared (or turn off program file comparison) click the field, and then click browse_button_small. Complete the
    Program File Compare Options
    dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal