Program Files Compare Options dialog box
How do I open the Program Files Compare Options dialog box?
- On the Schedules tab, select a Backup and Compare schedule containing an Allen-Bradley MicroLogix Controller, Allen-Bradley PLC-5 Controller, or Allen-Bradley SLC 500 Controller.
- In the lower left pane of theSchedulestab, select the Allen-Bradley MicroLogix Controller, Allen-Bradley PLC-5 Controller, or Allen-Bradley SLC 500 Controller contained in the schedule.
- In the lower right pane of theSchedulestab, click theProgram Comparefield and click
.
Use the
Program Files Compare Options
dialog box to specify which program files to compare for a particular asset in a Backup and Compare operation.
TIP:
You must have the RSLogix 5 or 500 programming software for your controller installed on the FactoryTalk AssetCentre client computer to configure these settings.
Provide Feedback