Data Files Compare Options dialog box

How do I open the Data File Compare Option dialog box?
  1. On the
    Schedules
    tab, select a Backup and Compare schedule containing an Allen-Bradley MicroLogix Controller, Allen-Bradley PLC-5 Controller, or Allen-Bradley SLC 500 Controller. If the schedule does not exist, create a schedule.
  2. In the lower left pane of the
    Schedules
    tab, select the Allen-Bradley MicroLogix Controller, Allen-Bradley PLC-5 Controller, or Allen-Bradley SLC 500 Controller contained in the schedule.
  3. In the lower right pane of the
    Schedules
    tab, click the
    Data Table Compare
    field and then click browse_button_small.
Use the
Data File Compare Option
dialog box to configure the comparison of data files for an Allen-Bradley MicroLogix Controller, Allen-Bradley PLC-5 Controller, or Allen-Bradley SLC 500 Controller.
TIP:
The compare report is generated, no matter whether there are differences found or not.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal