Find an asset in the asset tree
You can use the Find function to locate an asset in the asset tree.
To find an asset in the asset tree
- In the Asset View, select the container in which you want to search or select the root to search the entire tree.
- Click
in the Asset View , or select Edit > Asset Find. - Type all or part of the name of the asset you want to find.
- (Optional) Expand theOptionsbutton and select options for the search direction and whether you want to find whole words only.
- ClickFind Nextto find one instance of the search text in the tree. ClickFind Allto get a list of all instances of the search text in the asset tree.
Provide Feedback