Add an asset
Any asset you want the FactoryTalk AssetCentre system to manage must be included in the asset tree. On first use, all assets to be monitored must be added to the asset tree. The client computer must be connected to the FactoryTalk AssetCentre Server to add devices to the asset tree.
TIP:
If you add containers to your tree first, and set security for the containers, then assets you add within those containers will inherit the security settings of the container. This will save you time in setting security for your assets.
To add an asset to the tree you must have
Switch to Design mode
permission.You must also have the following permissions for the container into which you want to add an asset:
- Create Children
- Read
- Write
To add an asset to the tree
- Click
to enter Design mode. - If your asset tree is empty, you may first want to organize your asset tree with a useful representation of your plant.
- Click an asset in the Asset Catalog and drag it to the desired location in the tree.
- Fill out the information for the asset and clickOK.Assets (with the exception of File and Folder Item assets) are added to the tree as soon as theAddwindow for the asset opens. If you clickCancel, any changes made to the properties will not be saved, but the asset will still be added to the tree.
- Be sure to set security permissions for the asset. When initially added, an asset inherits the security settings of the container in which it is placed (and a container inherits the security settings of the container in which it is placed). Take advantage of this inheritance by setting security for a container before placing assets inside that container.
Provide Feedback