Container Properties dialog box
How do I open the Container Properties dialog box?
To show this dialog box, enter Design mode then right-click a container in the tree and select
Properties
. (If you are not in Design mode, and you have Read
permission, you will be able to view but not edit the properties.)Keyboard shortcut: Select the container and press
F4
.Use the
Properties
dialog box to view or change the properties of a container.When using this dialog box:
- To sort the properties alphabetically, click
. - To sort the properties by category, click
. - To change a setting, click the setting you want to change, and then select or type a new value.
- To change the size of any column, move the cursor over the line dividing the columns until you see a cross-bar shape, and then click and drag to expand or reduce the column size.
Provide Feedback