TIA Portal Addressing dialog box

How do I open the TIA Portal Addressing dialog box?
You can open the
TIA Portal Addressing
dialog box either while adding a Siemens S7 Controller (TIA Portal) to the asset tree or while editing a Siemens S7 Controller (TIA Portal)'s properties.
While adding a Siemens S7 Controller (TIA Portal) to the asset tree:
  1. If you are not already in Design mode, click design_mode_button.
  2. Drag a Siemens S7 Controller (TIA Portal) from the Asset Catalog to a container in the Asset View.
  3. Click anywhere within the
    Addressing Info
    field and click browse_button_small.
While editing a Siemens S7 Controller (TIA Portal)'s properties:
  1. If you are not already in Design mode, click design_mode_button.
  2. Double-click a Siemens S7 Controller (TIA Portal) in the tree.
  3. Click anywhere within the
    Addressing Info
    field and click browse_button_small.
Use the
TIA Portal Addressing
dialog box to provide the communication information necessary to connect to the Siemens S7 Controller (TIA Portal).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal