Add Allen-Bradley PowerFlex Drive dialog box
How do I open the Add Allen-Bradley PowerFlex Drive dialog box?
- If you are not already in Design mode, click
. - In the Asset Catalog, expand thePower Control Itemsnode.
- Drag an Allen-Bradley PowerFlex Drive asset onto the tree in the Asset View.
Use the
Add Allen-Bradley PowerFlex Drive
dialog box to add Rockwell Automation Motor Control devices (for example, PowerFlex drives and SMC controllers) as PowerFlex Drive assets to the asset tree. You can add an Allen-Bradley PowerFlex Drive asset in the root or in a container.The device is added to the asset tree as soon as this dialog box opens. Clicking
Cancel
in this dialog box abandons any changes made to the device properties, but leaves the device in the tree.AssetCentre provides two assets to backup Rockwell Automation drives: the Allen-Bradley PowerFlex asset type and the RA Drive asset type. When a drive is configured as an Allen-Bradley PowerFlex asset type AssetCentre uses the Universal Device Connector (UDC), from Connected Components Workbench, to perform the backup. The backup created by AssetCentre can be used in Connected Components Workbench. When a drive is configured as an RA Drive asset type, AssetCentre uses DriveExecutive Lite to perform the backup. The backup created by AssetCentre can be used in DriveExecutive Lite.
TIP:
It is not necessary to install either tool on the AssetCentre Agent computer; the AssetCentre installation process installs the necessary components.
If you are using Automatic Device Recovery (ADR) - that is to say, the drive configuration is managed through RSLogix 5000 or Studio 5000 Logix Designer – the drive configuration is part of the associated ACD file. When using ADR, there is no need to add either an Allen-Bradley PowerFlex Drive or an RA Drive asset to the AssetCentre system. The drive configuration is backed up as a part of the ControlLogix controller’s backup ACD file.
The following drives are compatible with Powerflex Drive:
PowerFlex 4 | PowerFlex 4M | PowerFlex 40 | PowerFlex 40P |
PowerFlex 400 | PowerFlex 400N | PowerFlex 400P | Multi-Drive 22-COMM-CNet |
Multi-Drive 22-COMM-DNet | Multi-Drive 22-COMM-ENet | Multi-Drive 1769-SM2 | PowerFlex 523 |
PowerFlex 525 | Multi-Drive PF52X Dnet | Multi-Drive PF52X E2P | Multi-Drive PF525 EENet |
PowerFlex 527 | PowerFlex 70 | PowerFlex 70 EC | PowerFlex 700 |
PowerFlex 700AFE | PowerFlex 700H | PowerFlex 700L | PowerFlex 700S |
PowerFlex 700S 2 | PowerFlex 700 AC | PowerFlex 700 VC | PowerFlex 6000T |
PowerFlex 7000 | PowerFlex 7000-2 | Kinetix 3 | PMM Deep Well |
PMM Deep Well HP | PowerFlex 753 | PowerFlex 755 | PowerFlex 755HiP |
PowerFlex DC | PowerFlex DC FC | MSR57 | SMC Flex |
SMC -50 | PowerFlex 755T | PowerFlex 755TM | PowerFlex 755TS |
PowerFlex 755TL | PowerFlex 755TR | PowerFlex 755CBI | PowerFlex 755TBS |
E200 Overload | E300 Overload |
As a general recommendation, Allen-Bradley PowerFlex Drive is the best asset type to backup your drives, EXCEPT the following drives which are only supported by RA Drive:
1305 Micro Drive (AC Drive) | 1305 Micro Drive (AC Drive) | 1336 PLUS Drive (SM) | 1336 PLUS II Drv |
1336E IMPACT | 1366R Line Regen | 1336T Vector (CNet) | 1336T Vector (PLC) |
1336T Vector (STD) | 1395 DC Drive | 1397 DC Drive | 160 Drive |
1756-DMD30 | 1756-DMF30 | 2364F -RGU | AC Drive |
Servo Drive | SMC DIALOG | SMP | FLOWSERVE IPS (200V) |
FLOWSERVE IPS (400V) | FLOWSERVE IPS (600V) |
Provide Feedback