Specify addressing information for Allen-Bradley PowerFlex Drive
You must be connected to the control network to specify addressing information for the device.
To specify the addressing information
- Click anywhere in theAddressing Infofield and then click
. Use the Select Device for Asset Typedialog box to browse the network for the Allen-Bradley PowerFlex drives that you want to add. When you have found the desired Allen-Bradley PowerFlex drive, select it and clickSelect. - Complete the remaining fields.
Provide Feedback