Add Allen-Bradley MobileView dialog box
How do I open the Add Allen-Bradley MobileView dialog box?
- To enter Design mode if you are not already in it, click
. - In the Asset Catalog, expand theSCADA, EOI and FactoryTalk Itemsnode.
- Drag an Allen-Bradley MobileView asset onto the tree in the Asset View.
Use the
Add Allen-Bradley MobileView
dialog box to add an Allen-Bradley MobileView operator interface to the asset tree. You can add an Allen-Bradley MobileView operator interface in the root or in a container.The device is added to the asset tree as soon as this dialog box opens. Clicking
Cancel
in this dialog box abandons any changes made to the device properties, but leaves the device in the tree.Provide Feedback