Items in Add Allen-Bradley MobileView dialog box
Items in the dialog box:
- (Parent)(Read-only) Shows the name of the container into which the Allen-Bradley MobileView operator interface is being added.
- Description(Optional) Type a description for the Allen-Bradley MobileView operator interface. The description will be shown in theArchivetab when the Allen-Bradley MobileView asset is selected. The description can be a maximum of 260 characters.
- NameEnter a unique and meaningful name for the device. This name will appear in the asset tree. The software defaults toAllen-Bradley MobileView. The name must be unique within the parent container. That is, you can have two devices with the same name in the asset tree, they just can't be in the same container. If you add a device into a container that already has a device of the same name, FactoryTalk AssetCentre will append a number (like_2) to the device name to ensure uniqueness.Asset names can be a maximum of 260 characters. The characters \ / : * ? " < > | are not allowed. The character pair &# is not allowed. A space, tab, underscore (_) or dollar sign ($) cannot be the first character in a name, but can be used elsewhere in the name. The following Microsoft Windows device names cannot be used as asset names, whether upper or lower case, with or without the colon: CON:, PRN:, AUX:, NUL:, COM1:, COM2:, COM3:, COM4:, COM5:, COM6:, COM7:, COM8:, COM9:, LPT1:, LPT2:, LPT3:, LPT4:, LPT5:, LPT6:, LPT7:, LPT8:, and LPT9. For example,Auxiliary Linewould be a valid name whereasAux Linewould not.
- Addressing InfoClick in this field and then click
to browse the network for the Allen-Bradley MobileView operator interface that you want to add. When you have found the desired device, select it and click Select. - Catalog InformationThe Rockwell Automation catalog number of the device to which you are (or will be) connected. If you browse for the addressing information as in Step 1 above, the catalog information will be filled in automatically.
- Configuration DataClick in this field and then click
to select the MER file for the device. This associates the MER file with the device in FactoryTalk AssetCentre and adds the file to Archive. - Device Name(Optional) Enter the name of the Allen-Bradley MobileView operator interface to which you are (or will be) connected.
- Firmware Revision(Optional) Enter the firmware revision of the Allen-Bradley MobileView operator interface to which you are connected.
- Hardware Revision(Optional) Enter the hardware series and revision of the Allen-Bradley MobileView operator interface to which you are connected.
- Hardware Serial Number(Read-only) The hardware serial number of the device to which you are connected. This is filled in automatically if the device selected in theSelect Device for Asset Typedialog box is valid.
- Hardware Type(Read-only) The type of device to which you are (or will be) connected. If you browse for the addressing information as in Step 1 above, the hardware type will be filled in automatically with MobileView Tethered.
- MAC Address(Read-only) The MAC address of the device to which you are connected. This is filled in automatically if the device selected in theSelect Device for Asset Typedialog box is valid.
- Manufacture Date(Read-only) The manufacture date of the device to which you are connected. This is filled in automatically if the device selected in theSelect Device for Asset Typedialog box is valid.
- Manufacturer(Read-only) The manufacturer is automatically filled in with Rockwell Automation - Allen Bradley.
- Series(Read-only) The series of the device to which you are connected. This is filled in automatically if the device selected in theSelect Device for Asset Typedialog box is valid.
- Warranty Number(Read-only) The warranty number of the device to which you are connected. This is filled in automatically if the device selected in theSelect Device for Asset Type dialogbox is valid.
- Agent GroupClick in this field and then click
to select the agent group for the device.- When adding the device under the root, the default value of Agent Group isSystem Default.
- When adding the device under a container, the default value of Agent Group isInherit from parent: the parent container’s Agent Group property.
- Asset Number(Optional) Enter an asset number for management or inventory purposes.
- Location(Optional) Enter information about the Allen-Bradley MobileView operator interface's location in your facility.
- Serial Number(Optional) Enter the Allen-Bradley MobileView operator interface's serial number.
- Properties Configuration(Optional) This box shows the number of default extended properties configured by theOptions dialog box: Extended Properties. To configure extended properties for the asset, click in this box, and then click
. In the Extended Propertiesdialog box, edit, add, or delete extended properties.
Provide Feedback