Specify addressing information for Allen-Bradley MobileView operator interface
You must be connected to the control network to specify addressing information for the device.
To specify the addressing information
- Click anywhere in theAddressing Infofield and then click
. Use the Selecting Device for Asset Typedialog box to browse the network for the Allen-Bradley MobileView operator interface that you want to add. When you have found the desired device, select it and clickSelect. - Complete the remaining fields as described below.TIP:You must have the RSLinx Enterprise orFactoryTalk Linxsoftware installed on the FactoryTalk AssetCentre client computer to configure these settings.
Provide Feedback