Items in Add Custom Device dialog box
Items in the dialog box include:
- (Parent)(Read-only) This field shows the name of the container into which the custom device is being added.
- Description(Optional) Type a description for the custom device asset. The description shows in theArchivetab when the custom device asset is selected. The description can be a maximum of 260 characters.
- NameEnter a unique and meaningful name for the device. This name shows in the asset tree. The software defaults toCustom Device. The name must be unique within the parent container. That is, you can have two devices with the same name in the asset tree, they just can't be in the same container. If you add a device into a container that has a device of the same name, FactoryTalk AssetCentre appends a number (like_2) to the device name to ensure uniqueness.Asset names can be a maximum of 260 characters. The characters \ / : * ? " < > | are not allowed. The character pair &# is not allowed. A space, tab, underscore (_) or dollar sign ($) cannot be the first character in a name, but can be used elsewhere in the name. The following Microsoft Windows device names cannot be used as asset names, whether upper or lower case, with or without the colon: CON:, PRN:, AUX:, NUL:, COM1:, COM2:, COM3:, COM4:, COM5:, COM6:, COM7:, COM8:, COM9:, LPT1:, LPT2:, LPT3:, LPT4:, LPT5:, LPT6:, LPT7:, LPT8:, and LPT9. For example,Auxiliary Linewould be a valid name whereasAux Linewould not.
- Backup DataSpecify the backup binder to use for Backup or Backup and Compare operations. FactoryTalk AssetCentre uses a binder to store backup files for custom devices. To specify a binder, click in this field and then click
. The Backup Data Browserdialog box opens.In most cases, when configuring a custom device for the first time, a backup binder does not exist yet. In this situation you can choose to leave Backup Data unspecified or specify a binder containing an empty folder.If you do not specify a backup binder, one is automatically created the first time a backup schedule runs for this device. The file name isAssetName_Backup, whereAssetNameis the name of the custom device asset as given in theNamefield in this dialog box. The new backup binder is placed under the custom device in the asset tree. The schedule is also updated to use the new binder.If you want to specify a binder containing an empty folder, create an empty folder on your computer or on a network location, and then use theBackup Datafield to add a binder specifying the empty folder as theSourceFolder. - Catalog Information(Optional) Enter the catalog number of the device to which you are (or will be) connected.
- Configuration DataClick in this field and then click
to select a binder for the device. This associates the binder with the device in FactoryTalk AssetCentre and adds the file to Archive. The binder should contain the project necessary for Backup or Backup and Compare schedules. - Device Name(Optional) Enter the name of the custom device to which you are (or will be) connected.
- Firmware Revision(Optional) Enter the firmware revision of the custom device to which you are (or will be) connected.
- Hardware Revision(Optional) Enter the hardware series and revision of the custom device to which you are (or will be) connected.
- Hardware Type(Optional) Enter the type of device to which you are (or will be) connected.
- Manufacturer(Optional) Enter the manufacturer of the custom device to which you are (or will be) connected.
- Agent GroupClick in this field and then click
to select the agent group for the device.- When adding the device under the root, the default value of Agent Group isSystem Default.
- When adding the device under a container, the default value of Agent Group isInherit from parent: the parent container’s Agent Group property.
- Asset Number(Optional) Enter an asset number for management or inventory purposes.
- Location(Optional) Enter information about the custom device's location in your facility.
- Serial Number(Optional) Enter the custom device's serial number.
- Arguments (<ARD>)(Optional) To configure the Arguments (<ARD>) for Backup (or Backup and Compare) schedules, click in this field and then click
. The Argument Editor - Backupdialog box opens. Enter the arguments and clickCheckin the dialog box to preview the final command line. Make sure that the folder or file location forArguments (<ARD>)is C:\Users\Public\RockwellSoftware\AssetCentre.TIP:To complete the final command line, you also need to specify theCommandandArguments (<ARG>)inOptions dialog box: Custom Devices. - Backup Location(Optional) Enter a name for a new backup folder, a path to a backup folder, or a path to an existing backup file. Make sure that the folder or file location forBackup Locationis C:\Users\Public\RockwellSoftware\AssetCentre.If you enter a name for a new backup folder, for example,New Backup.FactoryTalk AssetCentre creates a subfolder namedNew Backupwith the specified name in the backup location you designate inOptions dialog box: Custom Devices. The custom device backup files are stored in this new subfolder.If you enter a path to a backup folder, for example,C:\Users\Public\RockwellSoftware\AssetCentre\New Backup. The custom device backup files are stored in this designatedbackup folder.If you leave it blank, the custom device backup files are stored in the backup location you designate inOptions dialog box: Custom Devices.
- Custom ConfigurationThe configuration information of custom devices to which you are (or will be) connected. To browse the detailed custom configuration information, click in this field and then click
. The Custom Configurationdialog box opens. - Arguments (<ARD>)(Optional) To configure the Arguments (<ARD>) for compare operations, click in this field and then click
. The Argument Editor - Comparedialog box opens. Enter the arguments and clickCheckin the dialog box to preview the final command line. Make sure that the folder or file location forArguments (<ARD>)is C:\Users\Public\RockwellSoftware\AssetCentre.TIP:If theDevice Argument <ARD>item is not added into the right combo box in theCommand Editor - Backupdialog box, this field is not editable.To complete the final command line, you also need to specify theCommandandArguments (<ARG>)inOptions dialog box: Custom Devices. - Report LocationEnter a file name or a new path to store the compare report. Make sure that the folder or file location forReport Locationis C:\Users\Public\RockwellSoftware\AssetCentre.If you enter a name for a new report folder, for example,New Report. FactoryTalk AssetCentre creates a subfolder namedNew Reportwith the specified name in the report location you designate inOptions dialog box: Custom Devices. The custom device report files are stored in this new subfolder.If you enter a file name, for example,report.pdf. The custom device report file is stored in the report location you designate inOptions dialog box: Custom Devices.If you enter a path to a report folder, for example,C:\Users\Public\RockwellSoftware\AssetCentre\New Report. The custom device report files are stored in this designatedreport folder.You can also designate a path to a report folder by clicking
. Browse the folder to store report files, and then click OK.If you leave it blank, the custom device report files are stored in the report location you designate inOptions dialog box: Custom Devices. - Arguments (<ARD>)(Optional) To configure the Arguments (<ARD>) for post-backup operations, click in this field and then click
. The Argument Editor - Post Backupdialog box opens. Enter the arguments and clickCheckin the dialog box to preview the final command line. Make sure that the folder or file location forArguments (<ARD>)is C:\Users\Public\RockwellSoftware\AssetCentre.TIP:To complete the final command line, you also need to specify theCommandandArguments (<ARG>)inOptions dialog box: Custom Devices.
- Properties Configuration(Optional) This box shows the number of default extended properties configured by theOptions dialog box: Extended Properties. To configure extended properties for the asset, click in this box, and then click
. In the Extended Propertiesdialog box, edit, add, or delete extended properties.
Provide Feedback