Custom Configuration dialog box

How do I open the Custom Configuration dialog box?
  1. If you are not in Design mode, click design_mode_button.
  2. In the Asset Catalog, expand the
    Custom Device Items
    node.
  3. Drag a Custom Device asset onto the tree in the Asset View.
  4. In the
    Add Custom Device
    dialog box, navigate to the
    4. Backup
    section. Click in the blank field besides
    Custom Configuration
    , and then click browse_button_small.
Use the
Custom Configuration
dialog box to view and select the backup and post backup configuration of custom devices, in Design mode. (If you are not in Design mode, you cannot open or view this dialog box.)
TIP:
The backup and post backup configurations of custom devices are created in the Options dialog box: Custom Devices.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal