Select the custom device configuration
You can view and select the backup and post backup configuration of custom devices using the
Custom Configuration
dialog box.To select a custom device configuration
- Select a custom device configuration from theCustom Deviceslist in the left pane. The detailed information of backup and post backup configurations shows in the right pane.
- ClickOK. The selected custom device configuration is saved in theCustom Configurationfield of theAdd Custom Deviceand theDevice Propertiesdialog boxes.
Provide Feedback