Add Custom Device dialog box
How do I open the Add Custom Device dialog box?
- If you are not in Design mode, click
. - In the Asset Catalog, expand theCustom Device Itemsnode.
- Drag a Custom Device asset onto the tree in the Asset View.
Use the
Add Custom Device
dialog box to add a custom device to the asset tree. You can add a custom device in the root or in a container.The device is added to the asset tree as soon as this dialog box opens. Clicking
Cancel
in this dialog box abandons any changes made to the device properties, but leaves the device in the tree.Provide Feedback