Specify the backup binder or file if one does not exist in the asset tree

In most cases, when first configuring an asset, a backup binder or file does not exist yet. If you leave the backup binder for file unspecified, one is automatically created the first time a backup schedule runs for this asset. If you need to specify the backup binder or file, use the following steps.
To specify a binder
  1. In the left pane of the
    Backup Data Browser
    dialog box, select the asset you are configuring.
  2. Click the
    Add
    button.
  3. Fill out the
    Add Binder
    dialog box using the
    Source Folder
    field to specify a folder. Click
    OK
    . Once the binder is added to FactoryTalk AssetCentre, the
    Backup Data Browser
    dialog box is visible again.
  4. In the right pane of the
    Backup Data Browser
    dialog box, select the new binder and click
    OK
    .
To specify a backup file
  1. In the left pane of the
    Backup Data Browser
    dialog box, select the asset you are configuring.
  2. Click the
    Add
    button.
  3. In the
    Choose the File or Files to Add
    dialog box, select the file you want to specify. Click
    Open
    .
  4. In the right pane of the
    Backup Data Browser
    dialog box, select the new backup file and then click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal