Specify the backup binder if one exists in the asset tree
If the backup binder exists in the asset tree, you may want to specify the backup binder.
To specify the binder
- In the left pane of theBackup Data Browserdialog box, navigate to and select the device or container with the backup binder you want to add to this device.
- In the right pane, select the binder you want to add to the device.
- ClickOK. (Then clickOKin thePropertiesdialog box orAdddialog box.)
Provide Feedback