Unpin files or binders

Follow the steps to unpin files or binders.
Prerequisites
  • To unpin file or binder versions, you must have
    Pin
    permission.
To unpin a version
  1. Select
    View > Archive
    , or click the
    Archive
    button.
  2. In the asset tree, select the asset containing the file or binder to unpin, or select the file or binder with the version to unpin. If you select an asset, select the file or binder on the
    Archive
    tab.
  3. On the
    Archive
    tab, click the
    History
    tab or the
    Labels
    tab.
  4. At the bottom of the tab, select the version to unpin.
  5. Click
    Remove Pin
    . (If you don't see the
    Remove Pin
    button on the
    History
    tab, increase the size of the
    FactoryTalk AssetCentre
    window.)
  6. In the
    Remove Pin
    dialog box's
    Comments
    box, enter an optional comment with the reason for unpinning the version, and click
    OK
    . The maximum length for a comment is 2,500 characters.
    The pushpin icon pushbutton is removed from the version.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal