Check in files or binders automatically
You can set up FactoryTalk AssetCentre to automatically check in files when editing is completed and the file or editing software is closed. For binders, all the files are checked in when the key file is closed or the software for editing the key file is closed. This feature must be set for each file type that you want to check in this way (RSLogix 5 project files, Microsoft Word files, and so on).
Prerequisites
- To change the settings for automatic check-in, you must haveConfigure Personal Archive File Associationspermission orConfigure System Archive File Associationspermission.
To check in files or binders automatically
- SelectTools > Options, and then select theFile Associationscategory on the left.
- Select thePersonal Associationstab to change the settings for yourself or theSystem Associationstab to change the settings for everyone.
- ClickNewto add a new file type, or clickEditto change an existing file type.
- In theFile Associationdialog box, selectAutomatically check in file or asset after editingand specify theMonitor Type.
Provide Feedback