View file or binder history
Follow the steps to view file or binder history.
To view file or binder history
- SelectView > Archive, or click theArchivebutton.
- In the asset tree, select the file or binder for which you want to view the history. You can also select a folder to view when files were added or removed from it. If you select a device or container, no information or options will appear on theHistorytab; you must select a file or binder on theArchivetab to show history information.
- On theArchivetab, click theHistorytab.
If a version is listed in gray instead of black text, it means that version has been deleted because
Store latest version only
was selected.Provide Feedback