Meanings of the column headings on the History tab
The data in the following columns cannot be sorted. Change the width of a column by placing the insertion point between column headings and dragging the cross-bar shape.
- VersionA number assigned to the version of the file. Each file version created begins with the number 1. Each additional version, created by checking in changes or promoting a file or binder, is assigned a sequential number.
- TimeThe date and time an action was performed on the file or binder. The date will readYesterday,Today, or a specific weekday (likeWednesday) until seven days have passed. After one week, the date is shown in numeric month/day/year format (for example, 10/23/2007).
- ActionThe action performed (created, checked in, checked out, retrieved, pinned, promoted, or labeled).
- UserThe login ID of the user who performed the action on the file or binder.
- CommentsAny optional comments entered by the user who performed the action.
Provide Feedback