Promote files or binder version

Promote a version to the most recent version. This stores an old version of the file or binder as the most recent version and is useful when a previous version is now the one you want to use. Promoting a version also ensures that the promoted version will be the version other users retrieve when they get the file.
Prerequisites
  • To promote file or binder versions, you must have
    Promote
    permission.
To promote files
  1. Select
    View > Archive
    , or click the
    Archive
    button.
  2. In the asset tree, select the file or binder. If you select an asset in the asset tree, select the file or binder on the
    Archive
    tab.
  3. On the
    Archive
    tab, click the
    History
    tab or the
    Labels
    tab. These tabs allow you to promote different versions of the file or binder. For example, from the
    History
    tab, you could promote any checked-in version. From the
    Labels
    tab, you could promote any labeled version.
  4. Select the version to promote and then click
    Promote
    .
  5. In the
    Comments
    box, enter an optional comment explaining the promotion. The maximum length for a comment is 2500 characters.
  6. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal