View labels

Archive's
Labels
tab shows names used to describe a particular version of a file or binder. The
Labels
tab shows the version number and the time the label was added to a file or binder, making file or binder versions easier to identify at a later date.
To view labels
  1. Select
    View > Archive
    , or click the
    Archive
    button.
  2. In the asset tree, select the file or binder for which you want to view labels. To view labels, you can also select a device or container in the asset tree and then select the desired file or binder on the
    Archive
    tab.
  3. On the
    Archive
    tab, click the
    Labels
    tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal