Meanings of the column headings on the Labels tab
The column headings on the
Labels
tab include:- VersionA number assigned to the version of the file or binder. The first version created is numbered 1. Each additional version created by checking in changes to or promoting a file or binder is assigned a sequential number.
- TimeThe date and time a file or binder was labeled. The date will readYesterday,Today, orWednesday, etc. until seven days have passed. After one week, the date is shown in numeric day/month/year format (for example, 10/23/07).
- LabelThe label applied to this version of the file or binder.
Provide Feedback