Check out files and binders
Before modifying any file or binder stored in
Archive
, you must retrieve a copy of the file or binder to the current working folder on your computer. Retrieving a file or binder and making it available for editing is called checking out. Only one user at a time can check out a file or binder. If a file or binder is checked out by another user, you must wait until that user checks it in before you can check it out and edit it. However, you can get a file or binder that is checked out by another user so that you can view it in your project.If you check out an asset, you automatically check out all files and binders within the asset. Checking out a binder checks out all files within the binder. You have the option of checking out items located in subfolders of the asset (recursive check-out).
Prerequisites
- To check out files and binders, you must haveCheckOut - CheckInpermission for the asset.If theCheckOut does not require MoC workflowpermission is denied, you must submit the check-out request and get the approval from configured workflow approvers.
To check out files or binders
- SelectView > Archive, or click theArchivebutton.
- In the asset tree, select the asset containing the items to check out. Once you select an asset in the asset tree, you can also specify which files and binders to check out on theArchivetab.
- Click theCheck Outbutton on theArchivetab.If theCheckOut does not require MoC workflowpermission is denied, you must submit the check-out request and get the approval from configured workflow approvers.
- Complete theCheck outdialog box.
- ClickOK. A checkmark next to the file or binder in theArchivetab indicates the item is checked out. The location of the checked out item is also shown on theArchivetab.TIP:If you set file associations (that is, specify the programs used to edit different types of files), then when you open a file or binder from within FactoryTalk AssetCentre a message asks if you want to check out the file or binder.
Provide Feedback