Pin files or binders
Follow the steps to pin files or binders.
Prerequisites
- To pin file or binder versions, you must havePinpermission.
To pin a version
- SelectView > Archive, or click theArchivebutton.
- In the asset tree, select the asset containing the file or binder to pin, or select the file or binder with the version to pin. If you select an asset, select the file or binder on theArchivetab.
- On theArchivetab, click theHistorytab or theLabelstab.
- At the bottom of the tab, select the version to pin.
- ClickPin Version. (If you don't see thePin Versionbutton on theHistorytab, increase the size of theFactoryTalk AssetCentrewindow.)
- In thePindialog box'sCommentsbox, enter an optional comment explaining why the version is pinned and clickOK. The maximum length for a comment is 2,500 characters.Pinned versions are marked on theHistorytab with a pushpin icon
. If you pin a labeled version, that pinned file or binder is also marked on the Labelstab.
Provide Feedback