YAxis object (Trend object)
The YAxis object handles the vertical axis of the chart. The vertical axis represents the value of each pen.
The YAxis object supports the following properties:
The YAxis object supports the following constants:
Provide Feedback