ScalingLine property

Returns or sets which pen will control the scale of the chart if the ScalingOption property is set to rstLineScale. Read/write. Long.
Syntax
yaxis
.
ScalingLine
[
= value
]
where
yaxis
- is a YAxis object, or an expression that evaluates to a YAxis object.
value
- is a parameter of the type Long that specifies the number of the pen that controls the range. Pen numbers start with 1, not 0.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal