RSTminMaxOptions constants

The following constants are defined:
Constant
Description
rstAutoMinMax
Derives the range from the actual data.
rstCustomMinMax
Customizes the range for the chart by using the CustomMin and CustomMax properties.
rstPresetMinMax
Uses the range specified in the Min and Max properties of the pens.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal