CustomMaxName and CustomMinName properties
Returns or sets the display range at runtime by reading values from the container used by the trend object. Read/write. String
Set the MinMaxOption to rstCustomMinMax, and the Custom Min and/or Max Options to rstCustomMinMaxTag.
Syntax
yaxis
.CustomMinName
[ = name
]YAxis
.CustomMaxName
[ = name]
where
yaxis
- is a YAxis object, or an expression that evaluates to a YAxis object.name
- is a parameter of the type String that specifies the name of the tag.Provide Feedback