NumDecimalPlaces property

Returns or sets the number of decimal places shown on the y-axis scale. Read/write. Long.
Syntax
yaxis
.
NumDecimalPlaces
[
= value
]
where
yaxis
- is a YAxis object, or an expression that evaluates to a YAxis object.
value
- is a parameter of the type Long that specifies the number of digits to show after the decimal point. The range is 0 to 8.
Remarks
This property has no effect when the YAxis DisplayScale property is false.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal