IsolatedGraphing property

Returns or sets whether the chart lines are drawn in individual graphs or all in one graph. Read/write. Boolean.
Syntax
yaxis
.
IsolatedGraphingMode
[
= state
]
where
yaxis
- is a YAxis object, or an expression that evaluates to a YAxis object.
state
- is a parameter of the type Boolean that can be set to one of the following:
  • True
    . Displays each trend line separately
  • False
    . Displays all the trend lines together
Remarks
Plots each pen in a separate band of a trend chart.
tx_Isolated
Select isolated or non-isolated graphing on the Trend properties Y-Axis tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal