GSV/SSV Objects
When entering a GSV/SSV instruction, specify the object and its attribute to access. In some
cases, there will be more than one instance of the same type of object. Be sure to specify the
object name. For example, each task has its own TASK object that requires specifying the task
name to gain access.
IMPORTANT:
The SSV attributes must be uploaded to be saved to
the project.
IMPORTANT:
For the GSV instruction, only the specified size of
data is copied to the destination. For example, if the attribute is specified as a SINT and
the destination is a DINT, only the lower 8 bits of the DINT destination are updated, leaving
the remaining 24 bits unchanged.
IMPORTANT:
The alarm buffer was removed from the subscription
functions for alarming in the 21 firmware revision, and is no longer available. GSV
instructions that previously referenced the alarm buffer attribute are invalidated when
verifying the project. It is the responsibility of the programmer to correctly change any
application code that relied on this attribute.
FactoryTalk Design Studio
supports these GSV/SSV objects:Browsing for GSV/SSV objects
In
FactoryTalk Design Studio
, you can browse for available object attributes.- On the GSV or SSV instruction, right-click the backing tag, and then selectSelect Attribute.
- Select an object, and then select an attribute.
IMPORTANT:
The list of available scopes when browsing for an attribute may change depending on the
type of routine from which the attribute browser is launched.
When launching the attribute browser from an Execution-only routine, the Execution scope
is available, and the System scope is not. When browsing from a routine in a
System Object
, the System scope is available and the Execution scope is
not.Axis and Motion Group elements are accessed by selecting the System scope.
The Library scope, including
thisAOIDefinition
element, is browsable
only from routines or AOI logic in the Library explorer. AOI attributes can be accessed
outside of the Library explorer by typing
<object>.<attribute>
directly into the instruction
parameter field, where <object> in the name of the AOI definition to be referenced.Provide Feedback