ControllerApplication object
Attribute | Data Type | Instruction | Description |
|---|---|---|---|
SafetyStatus | INT | GSV | Status of the safety task. |
SafetyTaskFaultRecord | DINT | GSV | Record describing the most recent fault generated by the safety
task. |
SafetyLockedState | SINT | GSV | Non-zero when the safety task is locked and cannot be edited. |
SafetySignatureExists | SINT | GSV | Non-zero when a safety signature has been generated for the safety
task. |
SafetySILConfiguration | SINT | GSV | Safety Integrity Level (SIL) configuration of the safety
task. |
SafetySignatureIDLong | SINT | GSV | Extended long-form numeric identifier of the current safety
signature. |
SafetySignatureIDHex | STRING | GSV | Hexadecimal string representation of the current safety signature
identifier. |
SafetySignatureDateTime | STRING | GSV | Date and time at which the current safety signature was
generated. |
Attribute | Data Type | Instruction | Description |
|---|---|---|---|
majorEvents | UINT | GSV, SSV | Number of major fault log entries currently stored in the controller
fault log. |
majorFaultBits | UINT | GSV, SSV | Bitmask indicating which categories of major faults have occurred
since the last clear. |
minorEvents | UINT | GSV, SSV | Number of minor fault log entries currently stored in the controller
fault log. |
minorFaultBits | UINT | GSV, SSV | Bitmask indicating which categories of minor faults have occurred
since the last clear. |
Attribute | Data Type | Instruction | Description |
|---|---|---|---|
auditValue | LINT | GSV | Audit value used to detect unauthorized changes to the controller
program since the last download. |
canUseDefaultRPIFromControllerOutputParameters | USINT | GSV | When true, the default RPI for produced tags is derived from the
controller output parameters. |
controllerLogExecutionModificationCount | UDINT | GSV, SSV | Number of times the controller event log execution settings have been
modified. |
controllerLogTotalEntryCount | UDINT | GSV, SSV | Total number of entries currently stored in the controller event
log. |
controllerLogUnsavedEntryCount | UDINT | GSV | Number of controller event log entries that have not yet been saved
to non-volatile memory. |
dataTablePadPercentage | UINT | GSV | Percentage of extra memory reserved for data table growth to avoid
recompilation. |
inhibitAutomaticFirmwareUpdate | USINT | GSV, SSV | When true, prevents the controller from automatically applying
firmware updates. |
name | STRING | GSV | The name of this controller application. |
Provide Feedback