Device object

Identity
Attribute
Data Type
Instruction
Description
vendor
UINT
GSV
Deprecated. CIP vendor ID identifying the manufacturer of this device.
productType
UINT
GSV
Deprecated. CIP product type code classifying the general category of this device.
productCode
UINT
GSV
Deprecated. CIP product code uniquely identifying the device model within the vendor's product line.
productRev
UINT
GSV
Major firmware revision number of this device.
status
UINT
GSV
CIP Identity Object status word describing the current operational state of the device.
serialNumber
UDINT
GSV
Unique serial number assigned to this device by the manufacturer.
deviceName
STRING
GSV
Human-readable product name string for this device.
Module
Attribute
Data Type
Instruction
Description
entryStatus
UINT
GSV
Module entry status indicating whether the module configuration is complete and accepted.
faultCode
UINT
GSV
Fault code identifying the type of fault that has occurred on this module.
faultInfo
UDINT
GSV
Additional diagnostic information about the current module fault.
FirmwareSupervisorStatus
UINT
GSV
Status of firmware supervisor indicating whether the module firmware revision is compatible.
forceStatus
UINT
GSV
Bitmask indicating which I/O points on this module currently have forces applied.
instance
UDINT
GSV
CIP object instance number for this module within the Module Object class.
ledStatus
UINT
GSV
Bitmask describing the current state of the status LEDs on this module.
mode
UINT
GSV, SSV
Current operating mode of this module.
path
STRING
GSV
CIP path as a byte array identifying the route to reach this module on the network.
TimeSync
Attribute
Data Type
Instruction
Description
clockType
UINT
GSV
IEEE 1588 clock type identifier indicating the clock's role (e.g. ordinary, boundary, transparent).
currentTimeMicroseconds
LINT
GSV
Current IEEE 1588 system time expressed in microseconds since the PTP epoch.
currentTimeNanoseconds
LINT
GSV
Current IEEE 1588 system time expressed in nanoseconds since the PTP epoch.
domainNumber
USINT
GSV
IEEE 1588 PTP domain number that this device belongs to (0-127).
grandMasterClockInfo
GrandMasterClockInfo
GSV
Identity and clock quality of the current IEEE 1588 grandmaster clock.
isSynchronized
USINT
GSV
Non-zero when this device's clock is synchronized to the IEEE 1588 grandmaster.
localClockInfo
LocalClockInfo
GSV
Clock accuracy and variance characteristics of the local IEEE 1588 hardware clock.
manufactureIdentity
UDINT
GSV
Manufacturer-specific clock identity value for the IEEE 1588 implementation.
maxOffsetFromMaster
LINT
GSV, SSV
Maximum observed time offset from the grandmaster clock, in nanoseconds. Can be reset to 0 via SSV.
meanPathDelayToMaster
LINT
GSV
Mean propagation delay measured between this clock and the grandmaster, in nanoseconds.
numberOfPorts
UINT
GSV
Number of IEEE 1588 PTP-capable ports on this device.
offsetFromMaster
LINT
GSV
Current time offset from the grandmaster clock, in nanoseconds.
PTPEnable
USINT
GSV, SSV
When non-zero, IEEE 1588 Precision Time Protocol (PTP) is enabled on this device.
parentClockInfo
ParentClockInfo
GSV
Identity and port information of the current IEEE 1588 parent clock in the synchronization hierarchy.
portEnableInfo
PortEnableInfo
GSV
Enable or disable status for each IEEE 1588 PTP port on this device.
portLogAnnounceIntervalInfo
PortInfo
GSV
Log base-2 interval between IEEE 1588 Announce messages for each port.
portLogSyncIntervalInfo
PortInfo
GSV
Log base-2 interval between IEEE 1588 Sync messages for each port.
portPhysicalAddressInfo
PortPhysicalAddressInfo
GSV
MAC address and physical network address information for each IEEE 1588 port.
portProfileIdentityInfo
PortProfileIdentityInfo
GSV
IEEE 1588 profile identity (OUI and profile number) in use on each port.
portProtocolAddressInfo
PortProtocolAddressInfo
GSV
Network protocol address (e.g. IPv4) for each IEEE 1588 port.
portStateInfo
PortInfo
GSV
Current IEEE 1588 port state (e.g. master, slave, passive, listening) for each port.
priority1
USINT
GSV, SSV
IEEE 1588 BMCA priority 1 value; lower values indicate higher priority for grandmaster selection.
priority2
USINT
GSV, SSV
IEEE 1588 BMCA priority 2 value; used as a tiebreaker when priority1 values are equal.
productDescription
STRING
GSV
Manufacturer, model, and instance description of this IEEE 1588 clock device.
revisionData
STRING
GSV
Hardware and software revision data for this IEEE 1588 clock implementation.
stepsRemoved
UINT
GSV
Number of communication hops between this clock and the grandmaster clock in the IEEE 1588 hierarchy.
systemTimeAndOffset
SystemTimeAndOffset
GSV
Current system time and its offset from the IEEE 1588 epoch (TAI seconds since 1970-01-01).
userDescription
STRING
GSV
User-defined text description of this IEEE 1588 clock device.
CST
Attribute
Type
Instruction
Description
CSTCurrentValue
ULINT
GSV
Current coordinated system time value in microseconds since midnight January 1, 1984.
CSTCurrentStatus
UINT
GSV
Status flags indicating the current state and validity of the Coordinated System Time.
WallClockTime
Attribute
Type
Instruction
Description
WallClockTimeCSTOffset
ULINT
GSV, SSV
Offset in microseconds between wall clock time and the Coordinated System Time (CST).
WallClockTimeCurrentValue
LINT
GSV, SSV
Current wall clock time value expressed as microseconds since January 1, 1970 (Unix epoch).
WallClockTimeTimeZoneString
STRING
GSV, SSV
POSIX timezone string defining the local timezone rules including DST transitions for the wall clock.
WallClockTimeDSTAdjustment
INT
GSV, SSV
Daylight saving time adjustment in minutes currently applied to the wall clock time.
WallClockTimeApplyDST
USINT
GSV, SSV
Daylight saving time adjustments are automatically applied to the wall clock time.
WallClockTimeDateTime
DINT[7]
GSV, SSV
UTC-based Date/Time structure (Year, Month, Day, Hours, Minutes, Seconds, Microseconds).
WallClockTimeLocalDateTime
DINT[7]
GSV, SSV
Local Date/Time structure adjusted for time zone/DST.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal