MotionControlGroup object

The MOTION_CONTROL_GROUP object provides status information about a group of axes for the servo device. Specify the motion-group tag name to determine which MOTION_CONTROL_GROUP object you want.
These members are only available through the MOTION_SCHEDULER structure at runtime.
Templated Members
Attribute
Data Type
Instruction
Description
TaskMaximumScanTime
DINT
GSV, SSV
Task maximum scan time
TaskLastScanTime
DINT
GSV
Task last scan time
TaskLastIOTime
DINT
GSV
Task last I/O time
TaskMaximumIOTime
DINT
GSV, SSV
Task maximum I/O time
TaskAverageScanTime
DINT
GSV, SSV
Task average scan time
TaskAverageIOTime
DINT
GSV, SSV
Task average I/O time
Config Members
Attribute
Data Type
Instruction
Description
ControlGroupInstance
UDINT
GSV
Control group instance number
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal