Program object

The Program object provides status information about a program. Specify the program name to determine the Program object you want.
Attribute
Data Type
Instruction
Description
name
STRING
GSV
The name of this program as known to the controller.
instance
UDINT
GSV
The CIP object instance number assigned to this program.
lastScanTime
UDINT
GSV, SSV
Duration of the most recent scan of this program, in microseconds.
maxScanTime
UDINT
GSV, SSV
Maximum scan time recorded for this program, in microseconds. Can be reset to 0 via SSV.
inhibit
USINT
GSV, SSV
When non-zero, execution of this program is inhibited (disabled).
minorFaultRecord
DINT[11]
GSV, SSV
Array of 11 DINTs describing the most recent minor fault generated by this program.
majorFaultRecord
DINT[11]
GSV, SSV
Array of 11 DINTs describing the most recent major fault generated by this program.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal