Configuring storage containers
You can add storage containers individually or to the
Independent
Containers
group. When adding a container, a general description of the
container must be created before you can define the properties of the container. There are
three types of containers: Composite, Plug Flow, and Pallet.- Acompositecontainer holds more than one lot, but the lots are mixed. You cannot distinguish between lots, therefore the lot IDs do not matter, and you will not keep inventory on the lot. For example, a tank can be filled with one lot of milk. When another lot of milk is added, the two lots become mixed, and are, therefore, indistinguishable from one another.
- Aplug flowcontainer holds one type of material, but is comprised of two or more different lots. The first lot that went in is the first to come out. For example, you can add a lot of grain to a silo containing another lot of grain and the two lots remain separate (for the most part). Each lot can be inventoried.
- Apalletcan have multiple materials, which usually are bags of a specific quantity of material. For example, a pallet could be stacked with 100 pound bags of flour, sugar, and cocoa.Container information
Composite
Plug Flow
PalletDescriptionContains like materialContains multiple sublots layered in vesselContains multiple materials# of materials container may hold11n# sublots container may hold1nnAccess to sublotsSequentialSequentialRandomSublots trackable?No; anything added is combined with original sublotYes; assumption is that active sublot is at bottom of vesselYes; any sublot is always accessible
Provide Feedback