Changing inventory quantity
- From theEdit Material Storage Containerdialog, select theInventorytab. The list of sublots for the storage container displays.

- Select the record row to edit, and then click theEdit Distributionbutton. TheView Lot Distributiondialog opens.

- In theQuantitybox, type a new amount, and then clickOK.IMPORTANT:If you are changing a value that contains a decimal, use the Delete key to delete the value before typing a new value that contains a decimal. If you type over the old value containing the decimal, the new decimal is not recognized by the application.
Provide Feedback