Adding a new quantity of material to a deleted sublot

When a sublot of a lot of material is used up, the sublot is deleted from the database. You can create a new quantity of that same sublot, using the
Create Distribution
button.
  1. From the
    Edit Material Storage Container
    dialog, click the
    Create Distribution
    button. The
    Create Lot Distribution
    dialog opens.
    FTBMM_ED_Storage Container_Create Lot
  2. In the
    Label
    box, type a unique label name for the sublot.
  3. In the
    Quantity
    box, type the amount being distributed.
  4. In the
    Material Lots
    list, select a lot of material to distribute.
  5. Click
    OK
    to save the changes and close the dialog.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal