Configuring container inventory
The
Inventory
tab displays a view of the distribution of the lots of
material in the selected container. Each row represents a sublot. A sublot is an amount of
material in the selected lot that has been distributed to a container. The material, lot,
and label are used by the FactoryTalk Batch
Server when searching for a material to
bind to a recipe.When you edit, distribute, or delete a distribution in a container’s inventory, the results also affect the material’s inventory.
Provide Feedback