Distributing a lot

When you distribute a sublot of material, the distributed sublot appears with the
Label
,
Container
, and
Amount
distributed in the inventory of the selected storage container and also in the materials inventory.
  1. From the
    Edit Material Storage Container
    dialog, select the record row to distribute, and then click the
    Distribute
    button. The
    Distribute Lot
    dialog opens.
    FTBMM_ED_Storage Container_Distribute Lot
  2. In the
    Label
    box, type a unique label name for the sublot.
  3. In the
    Quantity
    box, type the amount to distribute.
  4. From the
    Storage Container
    list, select a container to use for storing the distributed amount.
  5. Click
    OK
    to return to the
    Inventory
    tab. If you distributed the lot into the container in which you are working, the new sublot displays, with the
    Label
    ,
    Container
    , and
    Amount
    distributed in the inventory.
    FTBMM_ED_Storage Container_Distribution
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal