Configuring container materials

From the
Materials
tab you can add or remove source materials, by group or individually, to the container.
  1. From the
    Edit Material Storage Container
    dialog, select the
    Materials
    tab.
    FTBMM_ED_Storage Container_Materials tab
  2. There are three methods you can use to move materials from the
    Source Materials
    list to the
    Configured Materials
    list.
    • To add a group of materials, select a group from the
      Source Materials
      list, and then click the
      Add Class
      button. All the materials assigned to that class are added to the
      Configured Materials
      list.
    • To add a single material, expand a material group to display the materials. Select a material, and then click the
      Add
      button.
    • To add all the source materials to the configured materials, click the
      Add All
      button.
  3. Click
    Apply
    to save the changes, or click
    OK
    to save the record and close the dialog.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal