Configure Batch objects
Right-click any Batch branch in
Preview
or Class View
, the Batch
configuration commands will appear at the applicable tree level.The following table describes each
Preview
command.Command | Description |
|---|---|
Add New | |
Add New Data Server | Creates data servers under the Data Servers node. |
Add New Enumeration | Creates enumerations under the Enumerations node. |
Add New Resource Class | Creates resource classes under the Resources Classes
node. |
Add New Tag Class | Creates tag classes under the Tag Classes node. |
Add New Process Cell Class | Creates process cell classes under the ProcessCell Classes
node. |
Add New Unit Class | Creates unit classes under the Unit Classes node. |
Add New Phase Class | Creates phase classes under the Phase Classes
node. |
Add New Process Cell | Creates process cells under the Process Cells
node. |
Add New Unit | Creates units under the ProcessCell . |
Add New Phase | Creates phases under the Unit . |
Contributing Instances | Highlights the corresponding instance in the Class View
for the Batch object selected in Preview . |
Refresh | Refreshes the Batch tree view. |
The following table describes each
Class View
command.Command | Description |
|---|---|
Add New | |
Add New Instance | Creates an instance under the selected object. |
Copy | Copies the selected object. |
Delete | Deletes the selected object. |
Export | Starts the Import Export Manager. |
Extract Attached Files | Extracts attached files to a location. |
Import | Starts the Import Export Manager. |
Navigate to Library | Navigates to the Batch library in the Registered Libraries
tree. |
Paste | Pastes a copied Batch object in the selected location. |
Paste Special | Displays the PasteSpecial window where child Batch objects
can be included or excluded. |
Refresh | Refreshes the Batch tree view. |
Rename | Renames the selected object. |
Update | Displays the Update Used Libraries dialog. |
View > Library Usage | Displays library usage details for the selected Batch
object. |
View > Library Details | Displays details of the library used to create the Batch
object. |
View > Referenced By | Displays details of objects that reference the selected Batch
object. |
Provide Feedback