Contribute instances

Use the
Contributing instances
menu to view and edit the properties of an object instance.
To contribute an instance
  1. In the
    Preview
    pane, expand
    Batch
    .
  2. Right-click a node shared by multiple instances, and then select
    Contributing instances
    .
    A list of contributing instances is shown.
  3. Select an instance.
    Its parameters property panel opens.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal