Add an instance

Use
Add New Instance
to add a library object instance to an existing library class in the
Class View
pane.
To add an instance
  1. In the
    Class View
    pane, right-click the library class from which the new instance will be created and then click
    Add New Instance
    .
    The
    Object Configuration Wizard
    is displayed.
  2. In
    Name
    , enter a name for the instance.
  3. (optional) In
    Description
    , modify the descriptive text to help identify the instance.
  4. (optional) On the
    Parameters
    tab, adjust the parameters as needed.
  5. Click
    Finish
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal