Generate an Area Model
Use the
Generate Area Model
menu to generate the Batch server Area Model file that
supports FactoryTalk Batch.To generate an Area Model
- InSystem VieworPreview, right-click a Batch server, and then selectGenerate Area Model.
- InSave As, specify the name and location of the Area Model file, and then selectSave.
- In theDocumentation Generationdialog, selectOK.
Provide Feedback